powered by CADENAS

Manual

Manual

10.5.4.5. Context menus

The context menus can be opened via Features in the history, as well as via sketch elements.

The breadth of the context menus depends on the respective feature.

The individual menu points are explained below.

[Note] Note

Subordinated features do not contain any other, but only less, menu points.

Change parameters: Launch context menu via construction step or sketch element

Change parameters: Launch context menu via construction step or sketch element

The context menu of a main feature basically contains the following five points:

Delete step : Removes the currently selected construction step.

A connection line shows the relationship between construction steps

A connection line shows the relationship between construction steps

[Note] Note

This variant only allows a reset, if the file has been saved, without taking over (this means including all others!) the construction steps / changes.