powered by CADENAS

Manual

Manual

13.4.2.  Create new set of rules

  1. Create an assembly configuration.

    Therefor, in the dialog area Project selection, on directory level, click on the context menu command New project. Enter a name. In the list field, select the option "Assembly configuration.prj". Confirm with OK.

    -> The configuration is created in the project selection area of PARTproject.

  2. In the context menu of the assembly configuration, click on the command Open with PARTdataManager.

    -> PARTdataManager opens.

  3. Enable the Configuration mode.

    -> Thereby the commands in the Configurator menu are enabled. (Otherwise they are grayed out.)

  4. In the Configurator menu, click on the command Show configurations and tables.

    -> Now the docking window Configurator becomes visible. The single dockings are still empty.

    Empty configurator

    Empty configurator

A detailed continuous example can be found under Section 10.7, “Example 1- Create a system of rules ”.