Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the following the characteristics / modeling rules will be described for each target system:
The parts must be located with the Z-axis to the top and with the Y-axis to the front (left in the isometric view)
The parts require the Placement Classification (see Section 5.9.2.4, “ Published element - Choose connection point ”)
The parts should be equipped with a changeable Level of Detail (also see below)
The parts must be classified with “Revit-Family-Templates” and “OmniClass 2006” (on this see separate point Classification below).
It is not allowed to use features / radius smaller than 1.4mm in modeling.
Use extrusion features and avoid rotation features - if possible.
Cut-rotations (e.g. chamfers) should also consider the 1.4mm tolerance
All kind of conductors, pipes, channels, etc. have to be modeled as “filled body” absolutely.
A REVIT placement point (Revit-Family-Template-Mapping) must be specified (please also see separate point Classification below).
For the placement in REVIT the axes of the REVIT placement point will be used for positioning /orientation. Take care that axes orientation of the point is according to the axes in REVIT (Z on top is recommended).
REVIT connection points always have to be in the geometric center of gravity of a planar surface (please also regard the orientation of the Connection Point).
The parts must be classified with IFC4
(See separate point Classification below.)
Use extrusion features – Avoid rotation features - if possible.
Absolutely avoid cut of edges (single edges should not touch each other):
It is not allowed to subtract volumina more than 1 time (cut features should not touch each other).
All parts should be tested with the “IfcCheckingTool”, see Further tests below.