powered by CADENAS

Manual

Manual

13.8.5. Create Assembly-Table-Project

In the hinge_asmtpl.prj context menu, you can find the command Create assembly table project .

Create assembly table project

Create assembly table project

The Create assembly table dialog box appears.

Select the project from the pull-down menu, which contains the table with which you want to control the assembly. In this example, it is HINGEDUMMY.

Create assembly table

Create assembly table

So far as the table "hinge_dummy" has been adjusted, the Standard name is correct; otherwise assign a definite standard name to the assembly.

Assign standard terms

Assign standard terms

So that only the Assembly-Table-Project is visible in the PARTdataManager, and not the "intermediary steps" template and assembly configuration, hide these with Hide project in the context menu of the directory tree. You should also hide the dummy project this way.

[Note] Note

Do not forget to update the index!

You can now select both single part, wing and bolt and the Assembly-Table-Project "hinge" in the PARTdataManager.

Assembly-table project - Parts view PARTdataManager

Assembly-table project - Parts view PARTdataManager

Assembly table project - Part view PARTdataManager

Assembly table project - Part view PARTdataManager

The assembly can now be committed to the CAD system as an Assembly-Table-Project (as in the example below, two times with L=50 and 2 differing angularities).

Assembly in Inventor

Assembly in Inventor

Assembly in Inventor

Assembly in Inventor