Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
3.15.2.
Add ERP-Mapping... / Edit ERP-Mapping...
3.15.2.1.
Change of folder
structure, project names and paths
|
|
---|---|
Prev | Next |
The folder structure of a catalog should not be fundamentally changed after the first publication. Especially a change of the structure and a change of the projects at the same time is very critical, because many end-media and interfaces base on the originally created structure. The “regular” add of new folders / projects is no problem. The same rule is also valid for the naming of the projects (NN/NB) – if they are changed the reference in the ERP system could get lost.
Change of folder structure -> See Section 6.9.3.1, “Interchanged lines - Expired lines”.
Change of project names -> See Section 6.9.3.3, “Change of project name”.
Also see above.