powered by CADENAS

Manual

Manual

13.5.1.1.1.1.  General
  • Description: The second expression in the Description field is the name used for the top level folder in the Configurator and Assembly dialog areas as soon as the newly applied assembly (* .prj ) is opened in the Configurator.

  • Standard name : You do not have to enter a standard name. You have the opportunity to set the name later using the CAD-system.

    [Note] Note

    Exception:

    If the assembly is used as Subassembly , the Standard name must be declared!

    If the Standard name is declared, it has to be unique !

    Syntax in general:

    *$name-of-part@Variable-of-part

    Example

    *$G382001@BESTELLNR._$G382001@F1.$G382001@F2.*

    See Section 10.9, “Example 3 - Create subassembly ”.

  • Measure unit : ...will be inserted automatically.

  • You have to enter Author, Company, Description and Last changed. Otherwise you can only leave this menu via Cancel

  • The License key is supplied by CADENAS , this field remains empty until the transfer of the assembly data to other persons.

    [Note] Note

    Every catalog has its own license!

    In order to open the catalog, the key must be filled out and the corresponding license must be present!