powered by CADENAS

Manual

Manual

9.5.3.1. Versioning system

Context menu at project level Context menu at directory level

The sub-menu command, Show status of the file, is only available at project level. Besides, the dialogs at project and directory level differ only marginally. In principle, the functions are the same.

[Note] Note

If under Extras -> Settings... -> General the option Update index after downloading catalog is set, the index becomes updated with every download process. If only one single subdirectory is downloaded, only the index for this directory becomes updated.

(Wait for the respective expenditure of time)