Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
"Physical" folder name for catalog
As the catalog name appears frequently at many different places, it is important to choose it short, clear and unique. E.g. at following locations this has to be considered:
Additionally it is important to always check if there is already a catalog with the target name existing at the mentioned places. It sometimes happens, that a supplier is CADENAS customer in different countries and of different subsidiaries. In such a case it should always be tried to create all data in one catalog. Only if this is really impossible, the catalogs should be separated with a name extension like „companyname_cn“ (e.g. for the chinese catalog), etc.
Catalog name - Catalog translation (Display name in PARTdataManager)
Beside the “physical” folder name (visible e.g. in PARTproject folder tree or Windows explorer) there is also a catalog name (see PARTproject > catalog main folder > tab General), which after translation (see PARTproject > catalog main folder > tab Translation), represents the finally shown name both in PARTdataManager, PARTcommunity and all other CADENAS end media.
Rules for the physical folder name
At least the first letter must always be a capital letter (even if the supplier has e.g. a small written name in the logo)
If possible also all further letters should be capital letters
Don’t include company types like “LLC.”, “S.A.R.L.”, “S.A.”, etc.
It has to be considered, that e.g. in case of asian companies, the name has to be translated into characters (like Kanji, etc.).
Also see Kennzeichnung von Katalogen.