powered by CADENAS

Manual

Manual

10.5.4.3.11.  Threads

The simultaneous core and nominal diameter display of thread is not possible in 3-D sketches, however it is required in the 2-D sketch derivation of the respective CAD program. Thread lines in PARTdesigner (Sketcher) are automatically applied as cosmetic elements during thread display.

[Note] Note

In the PARTdataManager the thread lines are invisible as a cosmetic element within the 3-D geometry. They appear only during the 2-D derivation of the part.

Screw with thread lines

Screw with thread lines

[Note] Note

If the buttons for creating a thread are not visible, activate the HistorySketcherWindow 'Threads' in the context menu of the toolbar.

HistorySketchWindow/Threads

HistorySketchWindow/Threads

[Note] Note

An example can be found in the training catalog under /partdesigner/gewinde.