powered by CADENAS

Manual

Manual

9.4.1. Symbols QA-status

For every directory level it is possible to Show description of QA steps in the context menu.

Show description of QA steps

Show description of QA steps

Not yet released

Pop-up window Legend

Pop-up window Legend

Released for editing (by customer)
Editing
Validated by editor
Automatic test passed
QA validation of team leader
QA validation of project leader
QA validation of customer

The levels of QA status show the project's progress and signalizes who is working on an issue!

The list shows the processes in the relation of customer - CADENAS. Detailed analyses with History analyzer show exactly which project took how long in which QA level. See also Section 6.8, “ History analyzer ”.

  Function

CUSTOMER

Check-in of data, DXF, TIF, BMP

Release of data

Editor (modelling)

Modelling and release of data for QA

PARTqaChecker

Check of data with PARTqachecker and release

QA

Check of data by QA team leader and release

Check of data by QA project leader and release

CUSTOMER

Check by customer and release on CD and Internet

The following table shows, when it is someones turn according to his role and which possibilities there are to change a status.

For example, in level 1 and 7 it is the customer's turn.

Changes of level 4 are set by automated tests.

In level 2 to 6, CADENAS is responsible.

QA stepsOverviewMatrix QA level - role

Matrix QA level - role