powered by CADENAS

Manual

Manual

13.5.1.5.1.  Properties

...opens the window Assignment of value range variables .

Variables of certain parts can be provided with value ranges instead of fix values. Value range variables are marked yellow in the table columns. (Section 8.5.2.6, “ Value ranges ”).

If a part with value range variables appears more than once in an assembly, it is reasonable to set each of them in an interdependence.

Modifying the length of one profile should lead to an automatic adoption of the second one. Therefor in the window Assignment of value range variables of P1 the assignment "KR1@L" has to be defined.

If the length L of the console pipe 2 was changed, length L of console pipe 1 was replaced by the same value.

Steps:

  1. Confirm setting with Return.

  2. Click Commit.

  3. Click OK.