powered by CADENAS

Manual

Manual

8.7.3.1. Building/editing class system

The context menu in the main window contains the following commands:

  • Add class...:

  • Add subclass...:

Via Add class... and Add subclass... you can build your class system.

  • Edit class...: At already existing classes make changes with Edit class...

  • Remove class: Deletes the class, not the class system.

[Note] Note

Only useful commands will be displayed. Upon starting the building of the tree structure for example, only Add class... is shown.

  • Parent class: Shows, if available, the name of the superordinated class.

  • Type: In the list field select the desired class type.

  • Internal id: Is automatically entered.

  • ID: Is automatically entered.

  • Name (<chosen standard language>):

    Enter the desired name. This term will be displayed in the class tree.

Finally confirm with OK.

Dialog box: Add class / Edit class

Dialog box: Add class / Edit class

[Note] Note

The commands Add class... and Add subclass... will call up the same window.

The dialog boxes in Edit class are also identical.

Example:

In the empty field -> context menu -> Add class...: ID "01" (already inserted), under "Name (german)" enter: "Bolts"

Context menu of "Bolts": Add subclass...: ID "01" (already inserted), under "Name (german)" enter: "Head cap bolts"

Context menu of "Bolts": Add subclass...: ID "02" (already inserted), under "Name (german)" enter: "Hexagon bolts"

Context menu of "Nuts": Add class...: ID "02" (already inserted), under "Name (german)" enter: "Nuts"

Context menu of "Nuts": Add subclass...: ID "01" (already inserted), under "Name (german)" enter: "Cap nuts"

Context menu of "Nuts": Add subclass...: ID "02" (already inserted), under "Name (german)" enter: "Hexagon nuts"

You will see the following outcome, for example:

Own classification system created

Own classification system created