Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Preliminary information about classifications:
Via classifications, alternative directory structures in the PARTdataManager are created. Into these directory structures (new) projects can be inserted. The allocation occurs via the individual classification fields (see below).
First click on the classification field then on the appropriate Browse button. --> The respective classification window opens. Assign the desired classifications. More detailed information can be found under Section 5.6, “ Add projects to classification ”.
The following classifications are available:
By Countries: classification according to countries in which each catalog company distributes products and/or owns subsidiaries.
See Section 7.8.2.5.1, “CNS classification and attributes ”.
eCl@ss is a standardized classification system for product groups and product attributes with the goal of enabling the electronic business of classified products.
eCl@ss is offered as a standard for information interchange between supplier and customers and is identified by a four-stage, hierarchical classification key with a keyword register consisting of 12,000 terms.
Features (eClass) : variables from the standard or company catalogs may be assigned to eCl@ss variables via the Class variables menu window. You can search for these eCl@ss variables later in PARTdataManager.
ICS - International Classification Standards:
The "International Classification for Standards" (ICS) is an international classification system, that compiles all economic sectors and activities which use technical standards.
The UNSPSC Standard is a product classification defined by the United Nations. The Standard represents a universal classification scheme for an extremely wide variety of product groups for worldwide use.