Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If you want to provide individual preview images for each table line then you can do this with the context menu command Create previews per line (value range fields are not considered).
Whenever parts of a project differ not only in size but also in form this is a great advantage.
Now, in the search results, you can recognize small differences already in the preview image, what makes part selection without large 3d preview easier.
The depiction in the CloudMap profits as well: The t-nuts right and top right would have been shown in one cluster only.
Furthermore the function is available in Cloud Navigator, Reports and Part comparison.
Preview images are created in PARTproject. The standard command for this is Generate image data/preview images further on. On this see Section 4.7.2.1.14.3, “ Generate image data/preview images ”.
For the creation of preview images per line use the command Create previews per line.
Since all graphics should have the same style no settings dialog is displayed at this place and the generation starts at once. When using a 64bit PARTproject the generation happens in several threads in parallel, what results in considerable time savings (especially for large catalogs).
Through the generation two additional files are created per project (.prj):
All preview images are arranged in one single png overall image. So less memory space is required.
Before publishing the preview images have to be created anew, whereby, thanks to GEOMDATE only the changed geometries are created. The QAchecker checks whether all preview images are up-to-date.
Compatibility to older PARTsolutions versions is given because in this case the new files are simply not used.