powered by CADENAS

Manual

Manual

8.5. Create technical previews / Dimensioning views

Dimensioning views may be made available in 3 different file formats:

  • *.3db

    With PARTdesigner, you can create Dimensioning views from the standard views, configure the dimensioning text against different sets of requirements and provide different additional versions for PARTdataManager.

    Details on this can be found under ???.

  • *.pra

    Normally Dimensioning views are provided by the customer in form of DWG/DXF files. In PARTproject, you can import them and convert to .pra.

    Details on this can be found under Section 8.5.2, “Import DWG/DXF files and convert them into .pra format”.

  • *.tif

    *.tif files can be created from paper catalogs by scanning, for example.

    Details on this can be found under Section 8.5.4, “*.tif files ”.

The respective views show up in the PARTdataManager in the Technical details window and can be opened with the Settings dialog.

Settings / technical details

Settings / technical details

[Note] Note

Dimension views may contain an image-table connection. On this see Section 5.5.5, “ Image-table connection ”.