powered by CADENAS

Manual

Manual

7.8.13. Tabbed page Image

The tabbed page Image only shows up at directory level.

Graphics which are then displayed as icons in PARTdataManager can be saved to catalogs and directories.

Do you want to import an image file?

  1. Precondition

    The preview defined on the General1 tabbed page under PARTserver preview is displayed in the index tree on the left side.

    [Note] Note

    The name of the Preview file has to be "katalog".

  2. Select the image in the tree.

    -> The image is displayed on the right side in the Preview section.

  3. Click on the Import button.

    -> The Explorer opens.

  4. Select the desired file and confirm with Open.

    Possibly a note shows up: "Do you want to overwrite the file?" Confirm with "Yes".

  5. Update the index via PARTproject, click on the icon Update index .

  6. --> The preview image is displayed in PARTdataManager now.

Do you want to edit the preview image?

  1. Select the desired image on the left side in the index tree.

  2. Click on the button Edit.

    -> The graphic program set for the respective file extension via Windows setting options is started.