Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The old project
splitinto2.prj
with
the value range
variable FORM shall be splitted into two
target projects splitinto2a.prj
and splitinto2b.prj
with a
fixed
variable FORM.
In this case, depending on the selection in the value range on the left side (old project), different target projects have to be opened on the right side. On this use Conditions.
Proceed as follows in order to perform mappings.
Check, whether all needed target projects are listed under Target project. (On this enlarge the dialog area.)
An automatic mapping has only been performed partly: The first target project has been automatically detected, however not the second one.
If not all needed ones are available, add them via Add target project .
-> The dialog box Search or select project opens.[41]
For each project, create a condition which controls the selection of the correct value.
In order to avoid a syntax error it is recommended to fetch a correct sample into the clipboard.
Therefore select a line and click on the context menu command Generate algorithm matching the selected line and copy it to clipboard (or on the same icon above alternatively).
In the dialog area Conditions click on the button Add condition .
Enter the saved syntax from the clipboard and adjust it accordingly.
For project
splitinto2a.prj
the condition is FORM.EQ.'A' and for project
splitinto2b.prj
FORM.EQ.'B'.
Repeat the procedure for the other project.
If now, in the left table (old version), the value of the value range variable FORM is changed, then automatically, in the right table (new version), the respective project with the correct fixed variable FORM is chosen.
If the switching is working correctly you can click on Verify all mappings .