powered by CADENAS

Manual

Manual

7.8.2.3.  PARTserver / PARTcommunity

[Note] Note

The PARTserver dialog area is displayed at directory and project level.

  • PARTserver preview :

    May be selected at project and directory level.

    As the preview (see illustration at right), the katalog.bmp set in the Image tabbed page box is displayed in PARTserver/PARTcommunity (online catalog system). If you wish to set a differing preview, enter this in the PARTserver preview field.

    [Note] Note

    In order to delete the set preview, it must be deleted manually from this field.

  • Thumbnail for PARTserver :

    Part image (2D and/or 3D) within the PARTserver/PARTcommunity detail level. (Project level)

  • Additional files :

    Visible at directory level.

    Enter those files here that should be copied after PARTserver/PARTcommuntiy. Per default the add-on ",0" is added.

    Should an entire subdirectory need to be copied (for ex., needed for assistants) however, then specify the subdirectory and change the parameter to "1".