powered by CADENAS

Manual

Manual

7.7.2.2.10.5. Project dependencies

With this function you create a diagram which displays project dependencies.

Prerequisite: Configuration file prjdependency.cfg -> Block Settings -> Key GENERATEDEPENDENCIESONINDEXUPDATE: Wert ='1'

Open the context menu command at project level.

PARTproject -> Context menu in directory tree at project level

Project dependencies

Project dependencies

For the display of the dependencies you have 3 options. Click on the desired one.

  • Show all dependencies

  • Show direct dependency only

  • Set custom dependency depth

Via the checkboxes, select which description the diagram is to contain.

  • Standard number

  • Norm text

  • Path

  • Name

  • Type

After all settings have been made, click on Generate diagram.