Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Draw the dimensioning line at the desired position and fix it by mouse click.
--> All dimensioning elements and the menu window Change parameter become visible.
Define the Offset value (dimension to reference axis) and the Height (Type size) of dimension (see fig.).
Default is "{AUTOMATIC%0}" with curly braces. (In the above example "%0", so that "8" without decimal places is displayed as dimensioning number.
"AUTOMATIC" takes the current value from the geometry. (Not recommended).
Define a static, dynamic or mixed static-dynamic Measure text.
Using %"number" you can define Decimal digits. (For example: A={A%2})
|
The new created view will be displayed in the "History" menu.
-> The dimensioning image is now available as 2D view in PARTdataManager.