Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The creation of a rotated pattern corresponds to the method of creating a pattern with equal orientation (see above).
The starting basis for the following commentary is a boring that is to be duplicated 12 times.
Via the button Choose new pattern origin... set the pattern origin on the desired boring.
Via Generate sketch on selected face. set a new sketch for the pattern.
In this sketch, set the point of origin for the construction of the pattern at the same place as the point of origin in the other sketch is located.
While holding down the CTRL button, select the button Rotate selection .
Adjust the values in the input fields Number, Rotation point and Angle of rotation and confirm with .
In the History mark Cut extrude and the sketch, which contains the pattern (in this example Sketch 3) and in the context menu, click Create pattern .
--> The borings are multiplied according to the pattern.
In the sketch, delete the circle and replace it with a square.
The bore holes are now arranged in squares and circles (but still equally oriented).