Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If you import a *.dxf file, the DXF Import window opens.
Filter of attribute/layer menu area:
In this field you will find a list of the layers of the import sketch and their assigned settings. Layers with the setting continuous are transferred into the PARTdesigner sketch. If you want to exclude layers/sketch elements from transfer to PARTdesigner, mark the respective layer row and in the option field, set a checkmark at Ignore belonging elements (more than one is possible in order).
Lines that cover each other are deleted before the sketch is imported.
Possible spaces between sketch elements are closed, since the sketch cannot be saved with interrupted contours in PARTdesigner.
Execute DXFHealer [64]
Via Execute DXFHealer you can activate the function directly upon import.
For the already imported sketch, use the button in the toolbar.
The following examples show the results of an error cleanup:
If changes have been made they will be announced in the message window. If nothing is announced, no changed have been made.
The following message ares possible, among others:
Note | |
---|---|
In order to adjust changes
according to your wishes, you can change the settings in the
configuration file under |
If
2 points have a smaller distance than pointEps
, they
will be considered equal. Through pointEps
the number
of the decimal places (in the example value below '3' [for
pointEps
, select
no values under 0,001]) has been set. For the midpoints of
arcs, more decimal points may occur.
pointEps=0.001
If
the difference between 2 angles is smaller than angleEps
degree,
they will be considered equal.
angleEps=1.0
If
a polygon has more than
corners that are located on a circle, then it is
advanced by a circle and/or arc.minVertexCountForArc
minVertexCountForArc=12
A
polygon chain must at least have the length minLinesForArc
in
order to be advanced by an arc.
minLinesForArc=4
An
element is seen as small, in other words it is removed it is
smaller than smallAbs
or than
smallRel
in
relation to the entire size.
smallRel=0.0001 smallAbs=0.1
Maximum distance to original (absolute and relative)
maxDistToOrigRel=0.0001 maxDistToOrigAbs=0.1
ABS are absolute values, REL is relative to size of part. If more is to be removed, then select the values larger. small<x> and maxDistrToOrig<x> should have about the same dimensions.