powered by CADENAS

Manual

Manual

8.7.2.4.1. Plate: Assign connection point (Drill) and butterfly screw

A plate is to be added to the start element butterfly screw via connection point Drill.

  1. Open the context menu of Drill in the Configurator menu.

  2. Select the menu item New rule… .

    --> The Rule properties window opens.

  1. In the Connection part field, all parts which may be connected, and contained in the Configurator dialog area are listed.

    If you mark one of these parts, their possible connection points are displayed in the Connection point field.

  2. Under Last name set a (unique) name for the rule.

  3. In the Connection part field, click on "butterfly screw" as well as in the Connection point field on expression "FS" and confirm your entries with OK.

    --> Dialog area Configurator: The connection is now displayed by a connection line between the two Connection points.

    --> Dialog area Assembly: The connection point boring has become part of the plate.

    --> The 3D preview shows the Connection point as a green triangle .

  1. Then, in Assembly open the context menu of the connection point boring.

  1. Select the menu item Rule 1 (ex.) insert.

    --> The butterfly screw is transferred into the assembly structure. As by the plate, the symbol is still crossed out , since there are still several characteristics.

  1. Click on the "butterfly screw".

  2. In the corresponding Table select a characteristic.

    --> The butterfly screw has been inserted into the Assembly. In the 3D preview it is located in the characteristic of the connection point boring, however it does not quite correspond to the diameter of the boring.