powered by CADENAS

Manual

Manual

14.2.  Context help...

The context help enables directly jumping in the according chapter.

  1. Click on the element with which you need help.

  2. Then either press Ctrl+F1 or click on the Context help... menu item.

    [Note] Note

    If the desired help page does not open at once, then please click on the same element a second time and then anew Ctrl+F1.

Help menu

Help menu

In the following some examples are given:

  • You have clicked into the input field of the Full-text search.

    Now click Ctrl+F1.

    -> The help opens at the adequate place.

  • The more specifically you click on a certain element, the more specifically the help opens.

    In the Settings dialog box select the checkbox Show small logos in project selection for example.

    Now click Ctrl+F1.

    [Note] Note

    Shouldn't be the display as desired, please check/uncheck again and then anew Ctrl+F1.

[Note] Note

You did not make a find with the context help?

Then please search with the default search or advanced search using terms. On this see under ???.