powered by CADENAS

Manual

Manual

6.9.5.1.  Change parameter

The displayed fields (in this case Base point X, Base point Y, Width, Height) of the Change parameter depend on the chosen feature. In this window, you can assign equations and variables as well as concrete values.

[Note] Note

Detailed information on mathematical functions and exact syntax can be found under Section 15.1, “PARTdesigner-Expressions ”.

Use the connected context menu (right-click into the respective field), in order to parametrize the respective sizes. Thus, variables, with the help of the menu points functions, operators, logic and Brackets can be connected to one another. Variables, functions, etc., are moved into the parameter field with a simple mouse-click and there attached to existing parameters.