Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Places a table element into sketch view.
The "Table" element is declared with "ELEMENT_" followed by a unique identification for the element.
[ELEMENT_table1]
The following attributes are available:
Concerns the text in the table cells. Compare Section 4.11.3.7, “[ELEMENT_text] Text ”.
Concerns the text in the table cells. Compare Section 4.11.3.7, “[ELEMENT_text] Text ”.
Indicates whether size or position may be changed in Edit mode.
The value of the key "column" is to be given as follows:
$2D_NR.=column width , $LINA.=column width , $2D_AMOUNT.=column width
The indication of the column width occurs in percent. The percent symbol is not to be given.
Example of a BOM table with declaration of Position number:
columns=$STKPOS.=10,$STKANZ.=10,$LINA.=120,$STKZCHN.=80
Detailed information on creation of position numbers can be found under Section 4.10.6, “Part-Annotation”.
List all column names separated by a comma.
columnames=Pos.,Anz.,Bezeichnung,Zeich / Artikel Nr.
Value range: top (alternatively no entry) | bottom
The specifications are important if the space indicated under "position_w" and "position_h" is larger than needed.
[ELEMENT_table1] type=table parent=frame position_x=55.80 position_y=69.53 position_w=145.92 position_h=104.97 tablename=BOM text_size=2 width_factor=0.5 sizeable=true columns=$2D_NR.=10,$LINA.=80,$2D_AMOUNT.=10 columnames=Nummer,LINA,Anzahl use_ratio=true align=bottom