Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
The calculation of the detailing occurs in the PARTdataManager, either automatically, based on a specific algorithm[45] or is set explicitly for each level of detail in PARTdesigner; these specific presettings are then incorporated into the PARTdataManager. |
The default setting for the display of the detailing in PARTdesigner is "High".
The following describes how you can individually configure the features display.
[45] The algorithm is based on an analysis of the relationship between the volume value of a detail and the entire volume of the part.