Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Last name: Per default "Base extrude xy" shows up. The numbers go up consecutively with each new extrusion.
You may change the name. However, use only ANSI characters (in other words: a-z, A-Z, 0-9 and spaces).
In the Length field you can set the measurement of the stretch of the 2-D object.
Against surface normal extruding means pulling into opposite sides. |
Both directions completes the extrusion along and against the plane normal. |
|
|
Draft : In order to create a draft from a 2-D sketch, enter the respective angle measurements into the draft field. |
You can connect a Condition to an extrusion as well. Possible characters are &, |, !=, =, >, <, >= and <=. |
Example: The sketch should only be extruded if for variable H (height) ea value larger than 10 has been set. |
Construction steps (features) which, based on their condition are excluded, will be deactivated in the history and identified by a -symbol.
In some rare situations we have the problem that we need to increase the accuracy for rasterization within the part to enable the creation of certain geometry. Therefore you can find this option for Base, Cut and Sweep.