powered by CADENAS

Manual

Manual

6.6.2.10.1.3.  Special adjustments

  1. Select the desired detailing in the pull-down menu (in this example "medium").

  2. Select a specific feature (in this example sketch 5), which you would like to add to / remove from this step.

    The activation/inactivation is shown by the checkmark in the command of the context menu.

    Visible in this configuration

    Visible in this configuration

    Visible in this configuration - activated

    Visible in this configuration - activated

  3. Result

    Differing from the PARTdataManager, the level of detail "medium" will now be additionally assigned to sketch 5.

    Sketch 5 invisibleThe example shows ISO 4231

    Sketch 5 invisible[a]

    Sketch 5 visible

    Sketch 5 visible

    [a] The example shows ISO 4231