Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
All visible in this configuration
This command is used, for example when you want to display the same feature at the "medium" level as with "high".
All invisible in this configuration
For adjustment this can be the quickest at level "low".
First, hide all features, and then show each feature bit by bit, using the "visible in this configuration" command (found at feature level), until you have reached the desired level of detail for your feature.
All settings are deleted with this.
If you want to select Levels of Detail, activate .
Possibly this is the fastest way to start over or simply to receive a "neutral" part.
Calculate configuration automatically...
Only now are the automatically calculated levels of detail available.
Via this command, the level of detail is automatically calculated and also saved in the 3DB. This can be used as the basis for further reductions.
Using this command, you can reestablish the initial state, in case you previously made any changes.
Deactivate automatic configurations
Use this option to make sure that the LOD is always set to "high" and exported as such independent of the LOD setting in the PARTdataManager.
Use this command if, for example, you want to use the level of detail "low" with "medium".