powered by CADENAS

Manual

Manual

6.6.3.3.1.2.  Polyline

Split polyline :

Polylines, such as for example occur when cutting two cylinders, are also split into "calculable" single segments with this function (circular arcs, ellipses, etc.).

As a group of single segments, the polyline can be edited and/or trimmed as well as imported to a CAD system with the "recognizable" properties.

In the example at the right (section highly zoomed in on) the Polyline can, for example be taken and cut via Cut element between 2 elements.

Scale drawing

After clicking on this icon, the Scale drawing dialog window opens.

Enter the desired value into the input field.

If desired, set the variable SCALE.

Confirm with OK.

The Change parameter opens. Here you can adjust the Scale factor and determine the Reference point.

 

The Change parameter window opens. Here you may adjust the Scale factor and determine the Reference point.