powered by CADENAS

Manual

Manual

6.13.2.  Physical properties of the part

  • Via this command you can see the physical properties of the respective part and calculate volume and center of gravity.

  • Via the Surface, Volume, Weight and Center of gravity list fields you can set the respectively desired Unit.

  • Material:

    • Either use the list field above

      or

    • select the checkbox Use for all single parts and assign the material for each part separately in the respective list fields.

[Note] Note

In the row of the single parts there is no multiplication with the amount of parts. The final result regards the amount.