Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Apply the order number as Standard variable in the part.
Note | |
---|---|
When exporting the part into the CAD system later, the respective Standard variables are found in the CAD system, in the file properties. |
Note | |
---|---|
You can also transfer the Standard variable CNSORDERNO via CNS classification into the CAD system. On this see Section 4.9.2.2, “ Menu item Variables ” (Variable with order number). |
In order to insert the Standard variable CNSORDERNO into the table proceed as follows:
Click on the button Standard variables.
-> The respective dialog box opens.
Activate the variables, which you want to overtake and confirm with OK.
-> Now the respective Standard variables are displayed in the list.
Close the dialog box Variable Manager by clicking on Ok.
-> Now the respective Standard variables are displayed in the table.
Instead of applying Standard variables in the table, you can apply the same variables as Class variables.