powered by CADENAS

Manual

Manual

12.1.3.  "Bill of material" tabbed page

By these fields you are able to create an external Bill of Material.

Command

Command line: this is where you define the program ("notepad.exe" in the example) to be launched as the "platform" for your Bill of Material. The placeholder "$BOMFILE 1 addresses BOMFile 1 and "$BOMFILE 2 addresses BOMFile 2 etc.

BOMFile 1, BOMFile 2 or BOMFile 3: Enter the name of the file in which the lower set content (from the applied program) should be read out. In the example, it is the content of variable column standard name "NB".

Choose Extras, Bill of material in order to display the contents. → The program is launched and the content is entered.