powered by CADENAS

Manual

Manual

4.10.6.1.  Mandatory parameters

Each part-notation must contain the following parameters:

  • ID

    ID is only required, if a dimensioning serves as Base dimension for a chain dimensioning.

  • Description

    The description is shown in the above listing. Initially a description is automatically given, when creating a new dimensioning, which can be adjusted as desired.

  • Type

    When creating a new dimensioning HORIZONTAL is automatically displayed. Adjust selection in the list field to PART-ANNOTATION. You can change the type anytime.

    [Note] Note

    The parameter fields are not updated until you have clicked Save changes .

  • Views

    At the desired 2D views, where the dimensioning shall be displayed, activate the checkbox.

  • Connection point

    The respective position number is placed close to the desired connection point.