powered by CADENAS

Manual

Manual

4.19.1. Renaming variables

[Note] Note

In order to rename variables, it does not suffice simply to change the name only in the table. The corresponding change must also be made in the geometry.

Such a change can be done "in one go" in PARTproject:

  1. Click with the right mouse button on the project file *.prj which contains the variable in question.

  2. Choose the Edit project in batch mode command in the context menu which opens.

  1. Choose the Rename variableoption in Settings.

  2. Enter the old name in the Variable namesfield and enter the new name in the New variable name field.

--> This is how to change the variable entry of the *.tab and the *.3db files!