powered by CADENAS

Manual

Manual

4.9.13.  Tabbed page Image

The tabbed page Image only shows up at directory level.

For catalogs or directories, images can be saved, which are displayed in PARTdataManager as additional icon.

Catalog level

Catalog level

[Note] Note

The image's name for the catalog itself should be catalog.bmp or catalog.png.

Subdirectory

Subdirectory

Do you want to import an image file?

  1. On the left, in the Project selection select the desired directory level.

  2. On the right under Edit project, select the tabbed page Image.

  3. Click on Import.

    -> The Explorer is opened.

  4. In the Explorer, choose the desired preview image and confirm with Open.

    Possibly a note is displayed: "Do you want to overwrite the file?" Confirm with "Yes".

    -> The image is displayed in the dialog area Preview on the right.

  5. Start PARTdataManager from PARTproject via context menu command Open with PARTdataManager.

    -> Now the selected preview image is displayed in PARTdataManager.

Do you want to edit the preview image?

  1. On the left, under Project selection, select the desired directory level.

  2. On the right, under Edit project, select the tabbed page Image.

  3. Click on the button Edit.

    -> The graphic program set for the respective file extension via Windows setting options is started.