powered by CADENAS

Manual

Manual

4.9.2.1.  General menu item

[Note] Note

The General menu item is displayed on project and directory level.

  • Project type :

    [Note] Note

    The setting option Project type is displayed at directory and project level.

    Click on the arrow in order to open the list field with the project types. Select the desired type from there.

    By selecting a type, a specific selection of tabbed pages shows up. You can find an overview on this under Section 4.9.1, “Overview on tabbed pages ”.

    Project types:

    Bitmap

    Project type Description

    2D project

    Create externally created 2-D drawings as project

    2D shell

    Drawings created with an older version of PARTsolutions

    3D project

    "Normal case" project

      Classification Search  

    3D bearing

    3D bearing project with several 3db files

    2D/3D project

    ...you are prompted later in PARTdataManager as to whether it is to be opened as a 2-D or 3D project

    2D/3D ball bearing

    ...is later asked for in the PARTdataManager whether it should be opened as 2-D or 3D project.

    Assembly configuration

    File created when saving a configuration in Configurator

    Assembly template

    Assembly template

    Project documentation

    *.doc, *.HTML and *.pdf files etc. are created in the form of a project

    Assembly table

    ...allows assemblies to be opened in PARTdataManager

    Directory

    Catalog directory (STANDARD etc.)

    PARTmedia

    Project on the basis of a PARTmedia file (a print catalog can be created from PARTsolutions parts with PARTmedia)

    Without geometry

    Assistant

    ...starts the PARTsolutions Web Wizard, which enables alternative masks for part selection to be displayed.

    See Section 3.1.6.4.13, “ Web Assistant (provided by customer) ” in PARTsolutions / PARTcommunity4Enterprise - User manual.

    Search Assistant

    Filter Assistant

    Global filter assistant created by administration. See Section 3.1.6.4.12.3.2, “ Search filter assistant (provided by PARTsolutions administration) ” in PARTsolutions / PARTcommunity4Enterprise - User manual.

    Calculation Assistant

  • Author :

    [Note] Note

    The setting option Author is displayed at directory and project level.

    Name of person that applied and/or is working on this project.

  • Company key :

    [Note] Note

    The setting option Company key is displayed at directory and project level.

    Basically you must enter the license key with which the respective folder (catalog) is secured against unauthorized access. On the highest level (for example: C:\Programs\partsolutions/23d-libs) this is not provided.

    [Note] Note

    If the entry is missing, you will receive a corresponding error message.

    .

    Error message - Saving without license key

    Error message - Saving without license key

  • Sorting of the directory :

    [Note] Note

    The setting option Sorting of the directory is only displayed at directory level.

    Choose the desired sorting in the list field.

    • Define sorting

      By selecting this option you can individually control the sorting.

      The variant Define sorting activates the setting that you have defined in the Sort directory context menu command at directory level.

    • Alphabetical sorting

      [Note] Note

      After these changes, you must update the index.

  • Short name (max. 16 characters) :

    [Note] Note

    It is imperative that a Brief Description is given and if available (based on selected project type) the Table file.

    The number character used should be oriented to the character limit of the "receiving" CAD system, since the short term is transferred as part name to the CAD during export.

    The short name must be unique and should preferably include the DIN number and the value of the variable "NENN" (represented with a placeholder) (e.g. “D1587_$NENN.”).

  • Row Label: ...is displayed highlighted in gray as the second column from the left in the table (see Fig. „ Row Label, characteristic attribute table, Preview “). This retains your overview as to what component attribute you are dealing with in the relevant row even when scrolling to the right (the columns with the important identification variables would be concealed).

    Information on the use of (translatable) text in the Row Label is found under Section 6.8.5.2, “ Translation functions”.

  • Similar to standard parts (optional):

    When cipping a catalog it is detected automatically, whether there are links to standards projects in NT, NN and NB. If this is the case, then the project is automatically assigned to the class of the found Standards project within the Standards classification.

    A manual entry here in the field Similar to standard parts (optional) results in the same.

    Projects classified in such a way are marked with the Standards icon in PARTdataManager.

    When using an ERP integration directories and projects can be colored based on role definitions in addition.

    Information on this is found under Section 4.12.2, “ Create and configure roles ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

  • The table file contains the Table, which you can see in the Part view of the PARTdataManager (see figure below). Set the respective file (*.tab, *.tac).

    [Note] Note

    If available (this is only the case for specific project types) the Table file must be specified.

  • Preview :

    Preview is the Image displayed in Part selection in the PARTdataManager (see illustration above). Likewise, in the Links side you can see the Part view (see illustration below). Enter the corresponding file (*.pra, *.bmp).

    Row Label, characteristic attribute table, Preview

    Row Label, characteristic attribute table, Preview

  • Product information pages:

    Under Product information pages, the catalog manufacturer can provide additional information ( e.g. installation information, shop info, etc.) for his catalog in HTML format. This can either be linked to a web site or being stored in a directory within the project directory. Variables can also be used. The syntax is the same as with document variables.

    Example:

    https://de.wikipedia.org/w/index.php?search=$NB.

    Information is displayed in PARTdataManager, in the Part view, respectively on a dedicated tabbed page. The view dynamically shows the respective row selection in table.

    1. At the option Product information pages, click on ....

      -> The same-named dialog box is opened.

    2. Click on and create the desired pages. With and you can edit and delete entries.

      Under Name enter Info 1 and under Address https://de.wikipedia.org/w/index.php?search=$NB. for example.

    3. Confirm with OK.

      -> In PARTdataManager, the created pages are displayed.

      Product information

      Product information

  • Additional export formats:

    Under Additional export formats, additional files (export formats) can be made available for the export (e.g. Revit [RFA = Revit Family Tables], EPLAN, DXF with special tool layers).[22]

    Example: Export in PARTsolutions

    Example: Export in PARTsolutions

    Additional files can be made available for the whole project, but also per row or value range value by adding a placeholder in the form of $VARIABLENAME..

    In the following you can a description on how to create the needed entries.

    1. Store needed export files in project directory.

    2. With a click on ... the respective dialog box is opened.

    3. Add the desired export files by clicking on . With and you can edit and delete.

      • ID: The internally used file name for the export.

        Examples:

        satfile2016
        rfafile2016
        dwgfile_left_view
        etc.

      • Description: Display name in Export menu of PARTdataManager

      • File name: When clicking on ... the Explorer is opened in the project directory for selection of desired files.

        Example:

        part.rfa

        or modified with variable

        part/%NAME..rfa

    4. Confirm with OK.

    5. Update index.

    6. Check result in PARTdataManager.

      Example: Export in PARTsolutions

      Example: Export in PARTsolutions

      In PARTcommunity the result looks like this for example.

      Example: Export in PARTcommunity

      Example: Export in PARTcommunity

  • Special case of General – projects without a table

    In the case of projects without table (such as document projects) fields Standard number (e.g. DIN 404) and Standard title (e.g. “Slotted capstan headed screw”) are also available.



[22] When using the Q&S import required entries are automatically created. Information on Quick & Simple can be found under Section 4.18, “ Create catalogs - Quick&Simple”.