The menu item
PARTserver/PARTcommunity is displayed at
directory and project level.
PARTserver preview:
May be selected at project and
directory level.
As the preview (see illustration at
right), the katalog.bmp set
in the Image tabbed page box is displayed
in PARTserver/PARTcommunity (online catalog system). If you wish
to set a differing preview, enter this in the PARTserver preview
field.
Note
In order to delete the set preview, it
must be deleted manually from this field.
Thumbnail for PARTserver:
Part image (2D and/or 3D) within the
PARTserver/PARTcommunity detail level. (Project
level)
Additional files:
Visible at
directory level.
Enter those
files here that should be copied after PARTserver/PARTcommuntiy. Per
default the add-on ",0" is added.
Should an
entire subdirectory need to be copied (for ex., needed for assistants)
however, then specify the subdirectory and change the parameter to
"1".