Dialog area Configurator: Open
the context menu of the rule "pipe clip"
(right-click).
Select Properties....
In the menu windows Rule properties activate the option
Reverse direction.
--> The pipe clip should look as
follows:
So that the pipe clip is
correctly positioned - in other words with the base plate on the
i-girder - it must still be moved half a clip part "H1/2" around base
plate "S2".
Dialog area Configurator: Again
open the context menu of the rule "pipe clip"
(right-click).
Select Properties....
In the Rule propertiesdialog window, right-click onTranslation.
Select Choose variable....
Define the
following: variable „S2“ and pipe clip „R“.
To expression "R@S2", add a
plus.
Define:
variable „H1“ and pipe clip „R“.
--> After
confirming with OK the pipe clip should be positioned
correctly.
--> After confirming with OK, the pipe clip is
now properly located on the i-girder.
This
concludes the example for creating a subassembly.