powered by CADENAS

Manual

Manual

5.4.1.2.2.  Optional parameters

  • Text

    Default value: {AUTOMATIC}

    You can find detailed information on all optional parameters under Section 5.4.1.7, “ Optional parameters ”.

  • Font height

    Default value: 3.5

  • Condition

    No entry per default

  • Arrow size

    No entry per default

  • Arrow factor

    No entry per default

  • Accuracy

    Default value: 1

  • Base dimension (Chain measurements)

    Enter the ID of the desired dimensioning as Base dimension.

    If the Base dimension cannot be created, then the second defined dimensioning substitutes the base dimension. If this neither can be created, then the third dimension substitutes the second, etc. In this way different dimensioning definitions can be set into the other (incremental dimensioning).

    [Note] Note
    • The first measurement in the chain (if defined as BBOX relative) must always be able to be created.

    • The base (superordinated) dimension has to be before subordinated dimensions.

  • Text shift (on the dimensioning arrow)

    [Note] Note

    The option is only available at the dimensioning type HORIZONTAL.

    The value determines the horizontal text shift from center.

  • Alignment

    [Note] Note

    The option is only available at the dimensioning types HORIZONTAL, VERTICAL and PARALLEL.

    Align dimensioning arrows / position dimensioning text

    Example

    Example

    In the list field, select one of the following values:

    • left

      The arrowheads show on the dimensioning lines from outside.

      The dimensioning text is located on the left dimensioning arrow.

    • center

      The arrowheads show on the dimensioning lines from inside.

      The text is centered on the arrow.

    • right

      The arrowheads show on the dimensioning lines from outside.

      The dimensioning text is located on the right dimensioning arrow.

    Align (automatic)

    • Checkbox deactivated: Alignment is considered in any case

    • Checkbox activated: Alignment is only considered, if the dimension does not fit between the arrows.

You can find detailed information under Section 5.4.1.7, “ Optional parameters ”.