powered by CADENAS

Manual

Manual

5.4.4.6. [ELEMENT_derivation] for one single derivation

The "Derivation" element represents a single 2-D derivation.

Valid derivations are the standard derivations (top, bottom, front, etc., and isometric).

The "Derivation" element is embedded into a box element.

The "Derivation" element is declared with "ELEMENT_" followed by a unique identification for the element.

Example:

[ELEMENT_derivation1]

The following attributes are available:

  • type=derivation

    Declares element type and is mandatory.

  • parent

    The derivation element adjusts its size according to parent element.

  • view

    The identifier of the standard derivation is entered here.

Example:

[ELEMENT_iso_view] 
type=derivation
parent=box2 
view=iso