Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In this section you can find details on the setting options of Derivation .
General: See Section 10.4.2, “General settings”.
Enter the key terms for the views to be displayed in the input field:
DW
templates are stored under $CADENAS_SETUP/layouts/2dderivation
.
You can find the template name in the section [Template] under the key "name".
[Template]
name=drawing_4_views_frame_DIN
Also see Section 5.4.4, “ 2D derivation: create own views ”.
Example: Setting 2 Rows, 2 Columns:
Shortened view is a special feature for catalogs which may look bad in the 2D derivation due to their proportions. This may happen with very long cylinders, for example. The 2D derivation would then appear to look more like a line than a cylinder.
If the part has an additional shortened view, then it is used (if activated).
Also see Section 14.2.2.4, “ Alternative 2D size Optimize drawing view on paper size / ” and Section 5.4.2, “ 2D derivation: alternatively shorted view ”.