powered by CADENAS

Manual

Manual

7.5.3.1. Apply new variable - Commit

  1. Right-click on the Variable field and enter the name of your variable.

    [Note] Note
    • The variable name may be maximally 10 Symbol long.

    • In order to keep the equations clear, the variable names should be as short as possible.

    • Only capital letters are to be used.

  2. With the TAB key or with your mouse, jump to the next Equation . Here you can give your variable a specific value. It is also possible to make the contents of this variable dependant on other variables, You can enter any equation into this field, for example 2* D1 or D1+D2. After confirming with Return the value is displayed next to the right of the variable in the Variable field.

    [Note] Note

    The degree of the angle functions must be set in parentheses.

  3. Since the variable name is only allowed to be 10 characters long, you may add a describing text about the variable into the Description field.

    [Note] Note

    In order for the variable to be later easily identified, a description should always be applied.

  4. Confirm you entries by clicking on the Commit button.

    The new variable is carried over into the variable list.

[Note] Note

Changes to equation values and description texts must be confirmed in the same manner.