powered by CADENAS

Manual

Manual

6.9.3.1. Interchanged lines - Expired lines

If lines have been interchanged or are not available in the new version anymore, an automatic mapping cannot be performed. You can recognize this at the respective icon in the table and in the directory tree. In this case the single suggestions have to be checked and confirmed line-by-line.

Example: The lines 1 and 2 have been interchanged, line 3 is not contained in the new version anymore, line 4 is line 3 of the old version and line 5 is unchanged.

Example: The lines 1 and 2 have been interchanged, line 3 is not contained in the new version anymore, line 4 is line 3 of the old version and line 5 is unchanged.

On the left side, select the lines one after another and on the right side, check the assigned line (blue arrow ).

If a line is correct, click on the icon Approve assignment .

If a line is not available in the new version anymore, click on the icon Revoke the mapping to this project .

Revoke the mapping to this project

Revoke the mapping to this project Revoke the mapping to this project

Assignment revoked

Assignment revoked

If all mappings are correct, click on the button Verify all mappings .