powered by CADENAS

Manual

Manual

7.5.1.4.5.2.  Rotate...

If you want to make a cut between 3-D solid and a 2-D sketch which occurs through the Rotation of the 2-D sketch, please do the following:

  1. Via New sketch... open the 2-D Sketcher and create a Circle as well as a Rotation axis .

  1. Do you want the extrusion of the body to completely penetrate the body or simply a certain length? Make the respective settings in the Rotational solid window.

In the example, the cuboid should completely be penetrated. In order to create a "total stretch" you must only confirm the Angle at 360°.

-> After confirming with OK both objects are cut. A circular tube is removed from the cuboid.

-> In the History another point (feature) shows up: Cut rotation .

The explanation of the other fields can be found here Section 7.5.1.4.4.1, “ Extrude... ”.