powered by CADENAS

Manual

Manual

5.11.2.  Import data / Create catalog

In PARTproject -> context menu of root directory -> Automation -> Batch import neutral formats (Quick and Simple), call up the settings dialog box.

[Note] Note

The license "ECATADDONS*NEUTRAL*IMPORTER" is required. If it is missing then the menu item Batch import neutral formats (Quick and Simple) is not displayed.

-> The same-named dialog box opens.

In the following the single setting options are explained:

  • Input

    • Directory: Determine the catalog source directory via browse button ....

      [Note] Note

      The name of the imported root directory determines the catalog name.

    • Structure of the CSV:

      By default, the CSV file should have been created with the following structure:

      • 1. row: Name of the table columns (Variable name)

      • 2. row: Description of the table columns

      • 3. row: Unit of the table columns

      • 4. row: Value of the table columns

        Characteristic attribute table in PARTdataManager

        Characteristic attribute table in PARTdataManager

      If the CSV file is exactly according to this scheme you do not have to perform any changes.

      If the CSV rows show another sequence then please adjust the sequence via arrow keys .

      Exemplary CSV file

      Exemplary CSV file

      Excel view of the sample CSV file

      Excel view of the sample CSV file

    • Recursive: If data shall be read from all directory levels then please activate this option.

  • Output: Required data

    • Directory:

      The Neutral catalog is automatically created under $CADENAS_DATA/23d-libs/<catalog name>.

      [Note] Note

      Catalog name is the name of the imported source directory.

    • Author:

      [Tip] Tip

      Please enter first the license key and afterwards the author.

    • License key:

      A standard license key with "QS" as catalog name looks like this, for example:

      CNS2009*CATALOGS*QS

      Corresponding entries in PARTproject are automatically set.

      PARTproject -> Edit project -> tabbed page General

      PARTproject -> Edit project -> tabbed page General

    • Part per project:

      Determine whether you want an own project for each part or multiple parts (characteristics) shall be combined in the table.

      • One part per project:

        Each project only contains one part (characteristic, meaning the table only one row).

      • All parts in one directory into one project:

        If there are several parts in the project directory then these are combined in a table with several rows.

        2 STEP files in project directory

        2 STEP files in project directory

        PARTdataManager: Characteristic attribute table with two characteristics

        PARTdataManager: Characteristic attribute table with two characteristics

    • Generate preview images (optionally)

      Select this option if there are no own preview images available. These are automatically created then. (This only applies for preview images of projects, not for preview images of directories.)

      If you use your own preview images then please regard that the option Generate preview images is activated.

  • Output: Optional data:

    Either define your own values by reference to variables of the CSV table or appropriate default values are automatically created.

    • No statement

      -> Default settings are used.

      • Standard number (NN)

        Default: Name of project directory is automatically used as Standard number (NN).

      • Standard text (NT)

        Default: No display of Standard title.

      • Standard name (NB)

        Default: Relative path of the input file.

        <Product group> - <Project> - <Document name>

        Catalog source directory with all directory levels

        Catalog source directory with all directory levels

        Display of LINA (BOM name) und NB (Standard name) in PARTdataManager

        Display of LINA (BOM name) und NB (Standard name) in PARTdataManager

      • BOM name (LINA)

        Default: Same as NB.

    • Specific statements

      If you use CSV files for the creation of your Quick&Simple catalog then you can use references to CSV file variables here.

      Excel view of the exemplary CSV file

      Excel view of the exemplary CSV file

      • Standard number (NN)

        You can refer to a variable of the CSV file (here exemplified $NNCUSTOM. with the value "Flange-Type1").

        The Standard number is displayed in PARTproject under -> Edit project -> Table file. See Fig. „ PARTproject -> Edit project -> Table file “.

        Furthermore the Standard number is displayed in PARTdataManager in the index tree.

        Standard number and Standard title in the index tree of PARTdataManager

        Standard number and Standard title in the index tree of PARTdataManager

      • Standard text (NT)

        You can refer to a variable of the CSV file (here exemplarily to $NTCUSTOM. with the value "Blank flange").

        The Standard title (=Standard text (NT)) is displayed in PARTproject under -> Edit project -> Table file.

        PARTproject -> Edit project -> Table file

        PARTproject -> Edit project -> Table file

        Furthermore the Standard title is displayed in PARTdataManager in the index tree.

        Display of Standard number and Standard title in PARTdataManager

        Display of Standard number and Standard title in PARTdataManager

      • Standard name (NB)

        Default: Relative path of the input file.

        You can refer to a variable of the CSV file (here exemplarily to $MATNR.).

        The Standard name is displayed in PARTproject under -> Edit project -> Table file.

        PARTproject -> Edit project -> Table file

        PARTproject -> Edit project -> Table file

        PARTdataManager: Display of NB and LINA

        PARTdataManager: Display of NB and LINA

      • BOM name (LINA)

        Here in the example in hand LINA also refers to $MATNR..

        QS-$MATNR.

    • The following features of the input CSV files are not imported into the table

      The following CSV file had been used, for example:

      Excel view of the exemplary CSV file

      Excel view of the exemplary CSV file

      With the help of this option you can prevent variables from being displayed in the characteristic attribute table:

      In the example in hand the table looks like this then:

      PARTdataManager: Certain columns (variables) hidden

      PARTdataManager: Certain columns (variables) hidden

      [Note] Note

      The variable NAME (document name) can not be hidden! Not even if no CSV files are used; it will always be displayed.

  • Start the generation by clicking on Ok.

    -> A generation log is displayed.

    Whenever parts could not be generated these are listed under Failed documents with an error description.

    The following functions are available now:

    Save log of the failed documents
    Import failed documents again
    Copy failed documents
    Move failed documents

Open your generated Quick&Simple catalog in PARTdataManager.