powered by CADENAS

Manual

Manual

7.5.1.  History

7.5.1.1. What are Features?
7.5.1.2. Part (name) context menu
7.5.1.2.1. Part information... (part)
7.5.1.2.2. Insert Fixed plane...
7.5.1.2.3. Exchange base planes (part)
7.5.1.2.4. Import foreign geometries
7.5.1.2.5. Dependencies... (part)
7.5.1.2.6. Search
7.5.1.2.7. Rotate (assembly)
7.5.1.2.8. Pan (assembly)
7.5.1.2.9. Mirror
7.5.1.2.10. Level of Detail
7.5.1.2.10.1. Configuration
7.5.1.2.10.1.1. Context menu commands
7.5.1.2.10.1.2. General adjustments
7.5.1.2.10.1.3. Special adjustments
7.5.1.2.10.2. Workflows
7.5.1.2.10.3. pdetailopt.cfg - Settings
7.5.1.2.10.3.1. Block MAIN
7.5.1.2.10.3.2. Block CONFIGNAMES
7.5.1.2.10.3.3. CATALOGS, DIRECTORIES, PROJECTS Blocks
7.5.1.2.10.3.4. Tabulation
7.5.1.2.10.3.5. Export of neutral formats and 2D derivation
7.5.1.3. Context menu base plane
7.5.1.3.1. Settings... (base plane)
7.5.1.3.2. New sketch... (base plane)
7.5.1.3.3. New 2-D sketch... (base plane)
7.5.1.3.3.1. Buttons in connection with New 2D drawing
7.5.1.3.3.1.1. Text
7.5.1.3.3.1.2. Polyline
7.5.1.3.3.1.3. ellipses
7.5.1.3.3.1.4. Insert hatch
7.5.1.3.3.1.5. Dimensioning mode
7.5.1.3.4. Dependencies... (Plane Feature)
7.5.1.3.5. Insert new plane... (Plane Feature)
7.5.1.3.6. Delete plane (Plane Feature)
7.5.1.3.7. Visible (Plane Feature)
7.5.1.3.8. Paste sketch
7.5.1.4. Sketch context menu
7.5.1.4.1. Edit...
7.5.1.4.2. Duplicate sketch
7.5.1.4.3. Construction sketch
7.5.1.4.4. Base
7.5.1.4.4.1. Extrude...
7.5.1.4.4.2. Rotate...
7.5.1.4.5. Cut
7.5.1.4.5.1. Extrude...
7.5.1.4.5.2. Rotate...
7.5.1.4.6. Copy (only sketch)
7.5.1.4.7. Cut (including dependencies) - Move complete history tree
7.5.1.4.8. Rename
7.5.1.4.9. Delete...
7.5.1.4.10. Show error...
7.5.1.4.11. Dependencies...
7.5.1.4.12. Visible in this configuration
7.5.1.4.13. Set mark
7.5.1.5. Extrusion and/or rotation feature context menu
7.5.1.5.1. Edit... (Base extrusion / Cut extrusion)
7.5.1.5.2. Show error... (Base extrusion / Cut extrusion)
7.5.1.5.3. Rename... (Base extrusion / Cut extrusion)
7.5.1.5.4. Delete... (Base extrusion / Cut extrusion)
7.5.1.5.5. Dependencies... (Extrusion feature)
7.5.1.5.6. Convert to cut / Convert to base
7.5.1.5.7. Set mark

Aside from the 2-D Sketcher, the History menu area is the central “scene of events” in PARTdesigner. Its context menus are used to open 2-D Sketcher and to create the components. In addition, the History documents all design steps, so that the relevant component structure can also be reconstructed and possibly modified at a later point.

Example

Open the Sketcher via the history

Open the Sketcher via the history