powered by CADENAS

Manual

Manual

4.8.2.4.  Variables

  • Preferred rows :

    Enter the Variable (column), which you want to define as the preferred row.

  • Transfer attributes via CNS classification:

    • Variable with order number :

    • Variable with mass

    • Material

    • Density [kg/m³]

    See Section 4.8.2.4.1, “Transfer attributes via CNS classification ”.

  • Order/Groups of Variables:

    See Section 4.8.2.4.2, “ Order/Groups of Variables - Hide columns (variables) ”.

  • Column visibility on PARTserver:

    Concerns the table display on PARTserver.

  • Variables containing graphics:

    If you want to display table rows with graphics (*.bmp) in projects, first apply a new variable/column in PARTeditor. The enter the file name of the desired graphic into a single row of the new column. Open the menu window Variable list in PARTproject (Browse ...) and activate the respective variable.

    [Note] Note

    Keep the graphic size low, because otherwise the operating speed of the system is restrained.

  • Variables with inch display:

    Column contents with metrical dimensions can be recalculated to inch dimensions per algorithm. Set the variables (columns) which are to be calculated thus.

  • Translatable Variables:

    Enter the text variables here whose fields contain translatable texts. Within the Translation tabbed page, store the respective translation text in the different languages. -> As soon as one sets another language for the program surface, the current field text is replaced by the alternative (foreign language) text.

    Detailed information on the subject "Translation" is found under Section 4.7.2.1.13, “ Translation ”.

  • Variable for Assembly positioning:

    Optional entry: Refers to "Testmeta".

    For the here indicated variables, certain tests are conducted for "Testmeta".

  • Variables containing external references:

    See ???.