powered by CADENAS

Manual

Manual

7.6.3.1.2.  Sketcher (conv.) tab page

[Note] Note

The conventional Sketcher Sketcher (conv.) should only be used for parts which were created with PARTsolutions V7.x.

  • Color settings :

    Set the colors for the different display elements in the conventional 2-D Sketcher. By clicking on the respective color button, a selection menu opens, in which the currently set color can be changed (see figure).

  • Show base points :

    Base points are especially helpful for circles and 3-point arcs. If you do not want the Base points of the given sketch elements to be displayed, deactivate the respective options.

  • Performance:

    • Show construction elements : All help elements noted in the Sketcher can be shown/hidden here.

    • Automatic switching : The End point of a line defined in the Create line window creates both the Start point for the line to be connected to it, if this option is activated.